Press

Here you can find out more about On Robot and our collaborative grippers. We welcome all enquiries from journalists and media agencies, and we look forward to getting in touch with you.

For general press and media enquiries contact:

 

Enrico Krog Iversen          Cezara Belciu

ENRICO KROG IVERSEN                           CEZARA BELCIU
Acting CEO                                                    Sales and Marketing Coordinator
+45 20 66 23 00                                           +45 22 63 83 09
eki@eki-management.dk                         cbe@onrobot.com

 

 

 

Odense, Danmark – 22. august 2017

On Robot lancerer ny griber, målrettet markedet for kollaborative robotter

Fleksibilitet, brugervenlighed og ekstraordinær tilpasningsevne er allerede veletablerede egenskaber der kendetegner griberne fra On Robot. Nu kommer så den nyeste griber, RG6, der udover de førnævnte egenskaber, også tilbyder større løfteevne og længere vandring til gavn for bearbejdning, materialehåndtering og emballering.
Read more

 

Charlotte, N.C. – August 22, 2017

On Robot Launches Next-Level Customizable Grippers for Collaborative Robots Tasked with MultI-size objects

On Robot, the fast-growing Danish manufacturer of innovative electric grippers for collaborative robots (cobots), today launched a flexible and energy-efficient gripper for cobots tasked with handling objects of various sizes. Easy to install on the arm of a cobot and simple to program, the RG6 is a bigger and stronger version of the company’s popular RG2, with higher payload than other two-finger collaborative grippers available on the market today. This higher adjustable force (25N to 120N) enables three times higher payload (6-8 kg or 13.2-17.6 lbs.) and wider stroke (160 mm or 6.3 in.), ideal for manufacturers automating the movement of delicate or heavy objects in applications such as pick and place, computer numerical control (CNC), machine tending, packaging and palletizing, and assembly.
Read more

 

 

June 20th, 2017

The board and investors behind the fast growing startup On Robot are recruiting a new CEO

Since a funding round in October 2016, when a list of significant investors added capital knowledge, and experience, the manufacturer of collaborative robot grippers, On Robot, has seen very strong growth during Torben Ekvall’s successful tenure as CEO. Over time, differing strategies on company goals and how to reach them have arisen, leading Ekvall to leave the company to pursue new ventures.

Investor and former CEO of Universal Robots, Enrico Krog Iversen, will serve as interim CEO until the company has found a successor.

We would like to thank Torben Ekvall for his contributions at On Robot.

Kind regards,

Lars Rønn
Partner, Vækstfonden Venture

For more information, please contact:
Enrico Krog Iversen
eki@eki-management.dk 
+4520662300

 

 

Gear manufacturing company Osvald Jensen decreases cycle time by 12 seconds using dual gripper from On Robot

The Copenhagen-based company has increased its productivity on their CNC machines by retrofitting them with RG2 Dual Grippers from On Robot that significantly decrease cycle times and allows for production to continue after operators have left the workshop.
Read more

 

Europaekspansion On Robot Pressemeddelelse

Industrien installerer flere og flere samarbejdende robot-arme. Det øger samtidig efterspørgslen på de fleksible, sikre og brugervenlige robot-gribere fra On Robot. Derfor forstærkes salgsorganisation nu med den erfarne salgschef Kenneth Bruun Henriksen. Med sin solide eksporterfaring skal han udbygge distributørnetværket i Europa yderligere. Produktionsfremgangen og medarbejdervæksten har desuden sprængt rammerne, og derfor er On Robot netop flyttet fra Odense Havn og ind i et større domicil i det sydvestlige Odense.
Read more

 

March 20, 2017, Charlotte, N.C.

ON ROBOT BRINGS INNOVATIVE, CUSTOMIZABLE GRIPPERS TO COLLABORATIVE ROBOT ARMS IN NORTH AMERICA

RG2 grippers bring extensive new capabilities for flexibility, ease-of-use, and customization; Danish company appoints Gary Eliasson as general manager in North America to continue aggressive global sales growth

On Robot, the fast-growing Danish manufacturer of innovative grippers for collaborative robots, is bringing its technology to North America to provide manufacturers with more user-friendly, safe and flexible grippers for collaborative robots (cobots). Officially launching to the North American market at Automate 2017 in April, On Robot’s two-finger RG2 grippers—available in both single and dual versions— mount easily on the arms of cobots without any external wires; for robots that have infinite rotation of the last joint, this enables unprecedented flexibility and productivity. The RG2 grippers can be easily programmed directly from the same interface as the robot, and the gripper can be modified without previous programming experience, making them ideal for collaborative robot users.
Read more