#ThoughtsOnRobots: Matteo Bardelli

Share
Collaborative Applications

In this interview with OnRobot, Product Manager Matteo Bardelli from Homberger shares his views on the future of collaborative applications.

For Matteo Bardelli from Italian system integrator Homberger, there is no doubt the worldwide pandemic will have an impact on the use of collaborative applications.

“I think the use of collaborative applications will grow in production environments due to the need for social distancing between workers. Also, we will probably see an increasing use of collaborative applications in workplaces with a high degree of human interaction, like fast food restaurants and toll booths.”

“Collaborative applications can be a direct help to fight Covid-19. A good example is in South Korea where they use collaborative applications to sterilize turnstiles in the subway stations. Also, there is  much potential for collaborative applications in research labs and hospitals where employees have a high risk of being infected.”

Simplicity and flexibility
According to Matteo Bardelli, the biggest advantages for collaborative applications are their simplicity and flexibility.

“Following the mass customization’s trend, productions must be scalable, reconfigurable, quick, and cost-effective. Collaborative applications have the ability to be meet these requests from the market.”

“Also, collaborative applications can be deployed fast which is a big advantage compared to industrial robots. Usually, the installation only needs some days, and the following process of perfecting and improving requires less than a month. After this period, the end user has a reliable and fully effective application that is productive 24/7.”

 

Should be truly collaborative
When deploying collaborative applications, it’s important to understand that they should be truly collaborative.

For the application to be truly collaborative, it’s important that it does a constant and repetitive task while the human operator’s job is to monitor the situation and analyze unexpected events.”

“Also, it’s essential that the operators accept the robot and don’t think it’s there to replace them. A good way to overcome this challenge is to transform the idea of the application from a machine that steals jobs to a powerful tool that is as essential in production as an electrical drill.”

 

Enhances strength points
According to Matteo Bardelli, a collaborative application works the best when it enhances the strength points of both the human operator and the robot.

“A good example is the inserting of batteries, which are usually heavy, inside drones. The robot handles the heavy weight, while the operator manually guides the arm to the correct position and by a touch tells the robot to end the task placing the battery.”

Looking forward, Matteo Bardelli sees an enormous potential for collaborative applications in all kinds of companies in the future.

“The world of collaborative applications has a high trust in innovation which means that every year is literally like a revolution. You can’t stop to study and be fascinated by this industry.”

 

-----------------------------------------------------------------------

#ThoughtsOnRobots

Share

Privacy Policy for processing and protecting personal data

This data protection policy applies to OnRobot.

The purpose of the policy is to ensure and document that OnRobot protects personal data in accordance with the rules for processing of personal data. The policy will also contribute to OnRobot providing information about its processing and use of registered personal data.

The policy will be reviewed each year.

Record of the processing of personal data

OnRobot processes personal data about:

  • Employees

  • Customers

  • Suppliers

  • Applicants

OnRobot has prepared a record of the processing of personal data. The record provides an overview of the processing for which OnRobot is responsible.

The personal data must be provided in order for OnRobot to enter into employment, customer and supplier contracts.

Purpose and lawfulness of the processing

Personal data are processed and archived in connection with:

  • HR management, including recruitment, hiring, dismissal and payment of salary

  • Master data for customers as well as orders and sales

  • Master data for suppliers as well as requisition forms and purchases

  • Contracts

Processing is legal by the authority specified in the appended record.

OnRobot does not use the personal data for purposes other than those listed. OnRobot does not collect more personal data than necessary to meet the purpose. 

Storage and erasure

OnRobot has introduced the following overall guidelines for storage and erasure of personal data:

  • Personal data are stored in physical folders.

  • Personal data are stored in IT systems and on server drives.

  • Personal data are not stored for longer than necessary to meet the purpose of the processing.

  • Personal data for employees are erased five years after employment has ended, and personal data about applicants are erased after six months.

Data security

Based on the appended risk assessment, OnRobot has implemented security measures to protect personal data:

  • Only employees with a work-related need to access the registered personal data have access to the data, either physically or via IT systems with rights management.

  • All computers are password protected and employees may not disclose their passwords to others.

  • Computers must have firewall and antivirus software installed, which must be updated regularly.

  • Personal data are erased securely in connection with phasing-out and repair of IT equipment.

  • USB flash drives, external hard disks, etc. containing personal data must be stored in a locked drawer or cabinet.

  • Physical folders are placed in a locked office or in locked cabinets.

  • Personal data in physical folders are erased by shredding.

  • All employees must be instructed in what to do with personal data and how to protect personal data.

 

Website and Cookie

  • The Personal Data Regulation allows you to treat personal data only legally for the purpose for which they have been collected. If you want to use data for purposes other than the original, you must always have the consent of the registrant.

  • Upon receipt of a business card from a customer you have his consent. If you write his information you need his signature on this paper to have a formal requirement for consent if you want to use his information. Then the customer allows OnRobot to use his data for purposes other than communication, upcoming promotions, product updates or further news including upcoming promotions, product updates and further news.

  • According to the Cookie Act, OnRobot must have the user’s consent to use this software on the user’s equipment. On The company’s intranet or similar closed group, the rules in the E-data protection directive do not apply.

Disclosure

Personal data about employees may be disclosed to public authorities such as the Danish Customs and Tax Administration and pension companies.

Processors

OnRobot only uses processors if they are able to provide the required guarantees that they will implement appropriate technical and organisational security measures to comply with personal data law. All processors must sign a processor agreement before processing commences.

Rights                                                                      

OnRobot safeguards the rights of data subjects, including the right to access, withdrawal of consent, rectification and erasure and will inform the data subjects of OnRobot’s processing of personal data. Data subjects are also entitled to appeal to the Danish Data Protection Agency.

Personal data breach

In case of personal data breach, OnRobot will report the breach to the Danish Data Protection Agency as soon as possible and within 72 hours. The manager is responsible for this reporting taking place. The report will outline the breach, the groups of persons affected and the impact the breach may have on these persons and how OnRobot has remedied or intends to remedy the breach. If the breach entails a high risk for the persons about whom OnRobot processes personal data, OnRobot will also notify these persons. OnRobot s will document any personal data breach on an access-controlled drive.

Erasure of data

The customer should assess when personal data need to be erased by asking the question:

When is it no longer necessary to store the personal data?

OnRobot follows the practice of the Danish Data Protection Agency:

Applications Are erased after 6 months in connection with job interviews. Unsolicited applications are erased immediately.
Employee data Are erased 5 years after termination of employment.
CCTV surveillance Is erased after 30 days.
Telephone conversations Are erased immediately or after up to 3 months.
Accounting records Must be stored for 5 years from the end of the financial year.


 

How to Grow your Business with Collaborative Applications
How to Grow your Business with Collaborative Applications
With the dawn of smarter, more adaptive tooling, robots can now function with greater speed, strength, safety and precision, accomplishing a wide range of tasks, while maximizing ROI. Learn more on how you can enable faster production at lower costs by downloading our free eBook.
GET THE FREE eBOOK
How to Grow your Business with Collaborative Applications