#ThoughtsOnRobots: Pascal Klee

Share
Collaborative robots- Pascal Klee

In this interview with OnRobot, Sales Manager Automation Pascal Klee from Müller Maschinentechnik shares his views on the future of collaborative applications. 

For Pascal Klee from the German Universal Robots distributor Müller Maschinentechnik, there is no doubt Covid-19 will have a big impact on the implementation of collaborative automation in the future. 

"I think the worldwide pandemic will result in more manufacturers turning to collaborative applications because they make it possible to maintain production in case of sickness of lockdown. Especially, the market will rise in the SME segment because smaller companies are often more flexible and open to new technology."

 

Deployed in 6-8 weeks

According to Pascal Klee, the biggest advantage for collaborative applications is that the applications are easy to use and fast to deploy in all kinds of production environments. 

"Collaborative applications are easy to program, and they can be deployed in as little as 6-8 weeks. Also, employees can work directly with the robots without fences or other precautions, and the robots are flexible and easy to move around which make them perfect for doing small batches. Another advantage is that collaborative applications have a fast ROI compared to industrial robots."

Involve workers from day 1

When deploying collaborative applications, Pascal Klee advice to involve the workers in the process from day 1.

"It's crucial for a successful implementation to talk to employees and involve them in the process. They are the ones that are going to use the application and it reduces their potential fear of the robot if they learn about the applications' possibilities before working with it. 

"Also, it's a good idea to start with a simple application and then scale up later. In that way, the company can learn the most about how collaborative applications work before moving on to harder automation tasks. The principle of KIS(Keep It Simple) is always a good way to start a project."

Get external advice

Pascal Klee recommends getting external advice from experts if nobody in the company has worked with automation before.

"Expert can help with estimating space requirements, deciding the right cycle time and speed, and choosing the right end effector. Also, experts can help planning the appropriate safety measures for the application."

Looking forwards, Pascal Klee sees great potential in both traditional applications like palletizing and machine loading and more innovative applications like OnRobot's 2,5D Vision System which offers depth perception for varying heights or stacked objects. 

"Collaborative automation is the future, and even though I have worked within the field a long time, I still get amazed about the applications and their ease of use. The potential is enormous."

-----------------------------------------------------------------------

#ThoughtsOnRobots

Share

Privacy Policy for processing and protecting personal data

This data protection policy applies to OnRobot.

The purpose of the policy is to ensure and document that OnRobot protects personal data in accordance with the rules for processing of personal data. The policy will also contribute to OnRobot providing information about its processing and use of registered personal data.
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
OnRobot has prepared a record of the processing of personal data. The record provides an overview of the processing for which OnRobot is responsible.
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
OnRobot does not use the personal data for purposes other than those listed. OnRobot does not collect more personal data than necessary to meet the purpose. 

Storage and erasure

OnRobot has introduced the following overall guidelines for storage and erasure of personal data:

  • Personal data are stored in physical folders.

  • Personal data are stored in IT systems and on server drives.

  • Personal data are not stored for longer than necessary to meet the purpose of the processing.

  • Personal data for employees are erased five years after employment has ended, and personal data about applicants are erased after six months.

Data security

Based on the appended risk assessment, OnRobot has implemented security measures to protect personal data:

  • Only employees with a work-related need to access the registered personal data have access to the data, either physically or via IT systems with rights management.
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
  • The Personal Data Regulation allows you to treat personal data only legally for the purpose for which they have been collected. If you want to use data for purposes other than the original, you must always have the consent of the registrant.

  • Upon receipt of a business card from a customer you have his consent. If you write his information you need his signature on this paper to have a formal requirement for consent if you want to use his information. Then the customer allows OnRobot to use his data for purposes other than communication, upcoming promotions, product updates or further news including upcoming promotions, product updates and further news.

  • According to the Cookie Act, OnRobot must have the user’s consent to use this software on the user’s equipment. On The company’s intranet or similar closed group, the rules in the E-data protection directive do not apply.

Disclosure

Personal data about employees may be disclosed to public authorities such as the Danish Customs and Tax Administration and pension companies.

Processors

OnRobot only uses processors if they are able to provide the required guarantees that they will implement appropriate technical and organisational security measures to comply with personal data law. All processors must sign a processor agreement before processing commences.

Rights                                                                      

OnRobot safeguards the rights of data subjects, including the right to access, withdrawal of consent, rectification and erasure and will inform the data subjects of OnRobot’s processing of personal data. Data subjects are also entitled to appeal to the Danish Data Protection Agency.

Personal data breach

In case of personal data breach, OnRobot will report the breach to the Danish Data Protection Agency as soon as possible and within 72 hours. The manager is responsible for this reporting taking place. The report will outline the breach, the groups of persons affected and the impact the breach may have on these persons and how OnRobot has remedied or intends to remedy the breach. If the breach entails a high risk for the persons about whom OnRobot processes personal data, OnRobot will also notify these persons. OnRobot s will document any personal data breach on an access-controlled drive.
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
How to Grow your Business with Collaborative Applications
How to Grow your Business with Collaborative Applications
With the dawn of smarter, more adaptive tooling, robots can now function with greater speed, strength, safety and precision, accomplishing a wide range of tasks, while maximizing ROI. Learn more on how you can enable faster production at lower costs by downloading our free eBook.
GET THE FREE eBOOK
How to Grow your Business with Collaborative Applications
Download Material
Please provide the following information to download the material.