OnRobot

D:PLOY Transferring - Your Automated Solutions for Pick & Place Applications

Get your robotic transferring (also known as Pick & Place) applications up and running in a few simple steps, with zero programming and zero simulations – all within a few hours. D:PLOY automates the manual process for building, running, monitoring and redeploying your Pick & Place application, saving more than half the time compared to conventional solutions.

Why D:PLOY Transferring?

Robotic transferring applications have never been faster or easier. Simply define part parameters and pick-and-place positions– D:PLOY automatically configures and optimizes your application for the best throughput. You get the same intuitive interface and monitoring dashboards for many light industrial or collaborative robot arms, running any transferring application, with fast and easy changes to meet dynamic production requirements.
At least 50% deployment time savings for faster ROI
Easily grow and manage new lines with fast re-deployment
Eliminate downtime and boost productivity
Relieve employees from monotonous tasks

Get started with D:PLOY Transferring in just a few easy steps

Step 1
Cell setup
D:PLOY automatically discovers most of the installed hardware. You no longer need to spend a lot of time on setting up the robot, install or program the interface to control tools and other cell components.
Step 2
Workspace
Use the intuitive graphical interface to set workspace obstacles and cell boundaries. D:PLOY automatically generates a collision-free path depending on the obstacles defined.
Step 3
Application setup
Enter workpiece attributes, pick position and other application inputs via the simple step-by-step flow. D:PLOY automatically generates and optimizes all the program logic, signal exchanges, event handling and path planning for the entire application.
Step 4
Operate and monitor
Run your application at a click of a button. With minimal configuration, get monitoring insights into performance indicators in real time to enhance productivity and minimize downtime.
Step 5
Re-deploy
Quickly make changes and re-deploy the application when production requirements change, such as introducing a new part or to meet new packaging or palletizing needs.

One System, Zero Complexity, Unlimited Opportunities

Up to 90% faster deployment
Fast and easy deployment
Zero programming

Multiple D:PLOY applications, same easy interface

The D:PLOY platform combines hardware and software to deliver solutions that address various robotic applications. Today, D:PLOY supports the following applications besides palletizing, with more to follow.

Palletizing
Quickly and easily set up and adapt your palletizing application with D:PLOY Palletizing
View solution
CNC Machine Tending
Eliminate the complexity of robotic CNC machine tending with D:PLOY CNC
View solution
Packaging
Get fast, easy packaging without complex robot programming with D:PLOY Packaging
View solution

How to build a transferring application with D:PLOY?

Learn how to build and run your transferring application with D:PLOY in this detailed video guide. You will be presented with the best practices, considerations, and main technical details needed to successfully deploy the application.
Start learning

Compatible with a wide range of robot brands

ABB Denso Doosan Elite Robots Epson Fanuc Hanwha Jaka Kassow Robots Kawasaki Robotics Kuka Nachi Omron Schneider Electric Techman Universal Robots Yaskawa ABB Denso Doosan Elite Robots Epson Fanuc Hanwha Jaka Kassow Robots Kawasaki Robotics Kuka Nachi Omron Schneider Electric Techman Universal Robots Yaskawa

Want to get started or have more questions about D:PLOY?

Our automation experts are ready to help you at every step!

Awards Won

RBR50 Robotics Innovation Award
RBR50 Robotics Innovation Award
DIRA Technology Prize
DIRA Technology Prize
Go Global Awards
Go Global Awards

How to Grow your Business with Collaborative Applications

With the dawn of smarter, more adaptive tooling, robots can now function with greater speed, strength, safety and precision, accomplishing a wide range of tasks, while maximizing ROI. Learn more on how you can enable faster production at lower costs by downloading our free eBook.
Get the free eBook